When the device is awake, it honors the conditions listed below:
- DATA Zero: If SDA is low and stable while SCL goes from low to
high to low, then a zero bit is being transferred on the bus. SDA can change while SCL
is low.
- DATA One: If SDA is high and stable while SCL goes from low to
high to low, then a one bit is being transferred on the bus. SDA can change while SCL is
low.
Figure 1. Data Bit Transfer on I2C Interface
- Start Condition: A high-to-low transition of SDA with SCL high
is a Start condition which must precede all commands.
- Stop Condition: A low-to-high
transition of SDA with SCL high is a Stop condition. After this condition is received by
the device, the current I/O transaction ends. On input, if the device has sufficient
bytes to execute a command, the device transitions to the busy state and begins
execution. The Stop condition should always be sent at the end of any packet sent to the
device.
Figure 2. Start and Stop Conditions on I2C Interface
- Acknowledge (ACK): On the ninth clock cycle after every address
or data byte is transferred, the receiver will pull the SDA pin low to acknowledge
proper reception of the byte.
- Not Acknowledge (NACK): Alternatively, on the ninth clock cycle
after every address or data byte is transferred, the receiver can leave the SDA pin high
to indicate that there was a problem with the reception of the byte or that this byte
completes the group transfer.
Figure 3. NACK and ACK Conditions on I2C Interface
Multiple ATECC608A-TNGLoRaWAN devices can easily share
the same I2C interface signals if the I2C_Address byte in the Configuration zone
is programmed differently for each device on the bus. Because all seven of the bits of the
device address are programmable, ATECC608A-TNGLoRaWAN can also share
the I2C interface with any I2C device, including any Serial
EEPROM.