The ECDH
command may use the value in TempKey as its
starting value for an ECDH
command. The ECC private key value in
TempKey must be generated by the GenKey
command. Once the TempKey has
been used by the ECDH
command, the TempKey.Valid flag is reset. If the
output is back to the TempKey location, then this flag will be set again.
Opcode |
Mode |
KeyId |
Data | Description | |
---|---|---|---|---|---|
Data 1 |
Data 2 |
||||
0x43 | 0x0D | 0x00 00 | X component of public key | Y component of public key |
|
0x0F | 0x00 00 | X component of public key | Y component of public key |
|
|
0x09 | 0x00 00 | X component of public key | Y component of public key |
|
|
0x05 | 0x00 0[Slot] | X component of public key | Y component of public key |
|
ECDH
command will be
encrypted in this mode. For the ATECC608A-TNGLoRaWAN the
ECDHPROT field is set to 0 and encryption will be dependent
upon the mode of the ECDH
command.Name | Mode | Size | Description |
---|---|---|---|
Response | 0x0D or 0x0F | 1 byte | Error code if command fails |
Response | 0x0D | 32 bytes | Shared Master Secret as clear text |
Response |
0x0F |
32 bytes |
Shared Master Secret as encrypted text |
Response | 0x05 or 0x09 | 1 byte | 0x00 if successful, otherwise an error code is returned |