Nonce
command must be run prior to the
first GenDig
command to load a value into TempKey. Subsequent
GenDig
commands will use the value stored in TempKey from the
previous GenDig operation.
Opcode |
Mode |
KeyID(1) |
Data |
Description |
---|---|---|---|---|
0x15 | 0x00 | 0x00 00 | — | Use Configuration Block 0 |
0x00 01 | — | Use Configuration Block 1 | ||
0x00 02 | — | Use Configuration Block | ||
0x00 03 | — | Use Configuration Block 3 |
Name | Size | Description |
---|---|---|
Response | 1 byte |
0x00 - If successful. Error code - If the command fails. |
32 bytes |
Configuration Zone Block |