In the example source code, the ADC result value is sent through USART to the serial terminal of the Data Visualizer and this serial terminal data is fed as input to plot the graph.
The data streamer protocol is used to send the ADC result to serial terminal.
How to use data streamer protocol to send 16-bit value:
The ADC has been configured for 10 bits and this 10-bit ADC result needs to be sent to an 8-bit USART. As one ADC result value will be sent as two bytes, a data streamer protocol has been used to send the ADC result to a serial terminal as below, so that one 16-bit value will be used to plot the graph.
USART_0_write(0x03); //START
USART_0_write(adc_data_LSB);
USART_0_write(adc_data_MSB);
USART_0_write(0xFC); //END
Data Visualizer Configuration:
.txt
file to be loaded in for
Data Streamer has configuration: D, 1, 1,
ADC0. To adjust the Y-axis in the graph, follow the points below: