To verify the ADC features, artificial noise can be generated with various methods and then this noise can be added to the input signal.
The example code to generate random noise:
unsigned int i;
unsigned int k;
unsigned char random_buf[512];
for (i=0;i<512;i++)
{
random_buf[i]= rand()%256;
}
dac_init();
while (1)
{
DAC.DATA = random_buf[k++];
if (k>512)
{
k=0;
}
}
random_buf[512]
is an array of random numbers 0 to 255 using
standard library function ‘rand()
’.
To generate a true random noise signal, sufficiently high DAC conversion rate is needed. It can be ensured by selecting the CPU clock frequency of the device which generates random DAC noise higher than the device using it as input noise signal.
The circuit illustrated in Figure 1 can be used to add noise to the signal to be measured.
For periodic noise, a PWM signal can be generated. To get the worst-case scenario of periodic noise in the test setup, the PWM frequency can be selected close to the ADC sampling frequency.
In the example source code, the default CPU clock is 3.33 MHz. ADC clock is 3.33 MHz/4 = 832.5 kHz.
In Free-Running mode, the sampling rate RS is calculated by:
So, RS is 832.5 kHz/13 = 64 kHz.
In the example source code, the PWM signal is generated with a 62 kHz frequency which is close to the ADC sampling frequency.