The user application (MiV_uart_blinky.hex
file) prints the status of the DDR3
read/write operation on the serial terminal through the UART interface.
Follow these steps to set up the serial terminal:
- 1.Launch Tera Term on the Host PC.
- 2.Select the identified COM Port in Tera
Term as shown in the following figure.
Figure 1. Identifying the COM Port
- 3.From the Menu bar, select Setup > Serial port... to set up the COM port.
Figure 2. Setting Up the Serial
Terminal
- 4.Set the Speed (baud) to 115200 and Flow Control to none and
click OK as shown in the following figure.
Figure 3. Setting Up the Baud Rate
After the serial terminal is set up, next step is to program the RT PolarFire device.