AT13481

Function freqm_enable_callback()

Enable an FREQM callback.

enum status_code freqm_enable_callback( struct freqm_module *const module, const enum freqm_callback_type type)

Table 1. Parameters
Data direction Parameter name Description

[in, out]

module

Pointer to the software instance struct

[in]

type

Callback source type

Returns

Status of the callback enable operation.

Table 2. Return Values
Return value Description

STATUS_OK

The callback was enabled successfully

STATUS_ERR_INVALID_ARG

If an invalid callback type was supplied