SAM-ICE has a JTAG connector compatible to ARM’s Multi-ICE. The JTAG connector is a 20-way Insulation Displacement Connector (IDC) keyed box header (2.54mm male) that mates with IDC sockets mounted on a ribbon cable.
The table below lists the SAM-ICE JTAG pinouts.
Pin | Signal | Type | Description |
---|---|---|---|
1 | VTref | Input |
This is the target reference voltage. It is used to check if the target has power, to create the logic-level reference for the input comparators and controls the output logic levels to the target. It is normally fed from VDD on the target board and must not have a series resistor. |
2 | Vsupply | NC |
This pin is not connected in SAM-ICE. It is reserved for compatibility with other equipment. Connect to VDD or leave open in target system. |
3 | nTRST | Output |
JTAG Reset. Output from SAM-ICE to the Reset signal on the target JTAG port. Typically connected to nTRST on the target CPU. This pin is normally pulled HIGH on the target to avoid unintentional resets when there is no connection. |
4 | GND | - | Common ground |
5 | TDI | Output |
JTAG data input of the target CPU. It is recommended that this pin is pulled to a defined state on the target board. Typically connected to TDI on target CPU. |
6 | GND | - |
Common ground |
7 | TMS | Output |
JTAG mode set input of target CPU. This pin should be pulled up on the target. Typically connected to TMS on target CPU. |
8 | GND | - |
Common ground |
9 | TCK | Output |
JTAG clock signal to target CPU. It is recommended that this pin is pulled to a defined state on the target board. Typically connected to TCK on target CPU. |
10 | GND | - |
Common ground |
11 | RTCK | NC |
Input Return test clock signal from the target. Some targets must synchronize the JTAG inputs to internal clocks. To assist in meeting this requirement, a returned and re-timed TCK can be used to dynamically control the TCK rate. SAM-ICE supports adaptive clocking, which waits for TCK changes to be echoed correctly before making further changes. Connect to RTCK if available, otherwise to GND. |
12 | GND | - |
Common ground |
13 | TDO | Input |
JTAG data output from target CPU. Typically connected to TDO on target CPU. |
14 | GND | - |
Common ground |
15 | RESET | I/O |
Target CPU reset signal |
16 | GND | - |
Common ground |
17 | - | NC |
This pin is not connected in SAM-ICE |
18 | GND | - |
Common ground |
19 | - | NC |
This pin is not connected in SAM-ICE |
20 | GND | - |
Common ground |