Multi-core debugging requires multiple debuggers or multiple instances of the same debugger. Two or more debuggers can use the same SAM-ICE simultaneously. Configuring a debugger to work with a core in a multi-core environment does not require special settings. All that is required is proper setup of the scan chain for each debugger. This enables SAM-ICE to debug more than one core on a target at the same time.
The following figure shows a host, debugging two CPU cores with two instances of the same debugger.
Both debuggers share the same physical connection. The core to debug is selected through the JTAG settings as described below.