Figure 7-2 shows the phase voltages of the
windings by the 3-phase BLDC in both sinusoidal drive and trapezoidal drive. Three
oscilloscope probes are connected to the voltage dividers of each motor winding. The
difference between the driving phase voltages can be observed. The sinusoidal drive
produces a saddle shape waveform where the switching voltage is smoothly varied. The
trapezoidal drive, on the other hand, generates a trapezoidal waveform.
Figure 1. Phase Voltages
Using a current probe, the phase current of the trapezoidal and sinusoidal
current drive is obtained and shown in Figure 7-3. Both drive runs at 2400 RPM. Ripples
are observed in trapezoidal drive. The sinusoidal drive provides a smoother line current
compared to the trapezoidal drive. Ripples are more apparent in the trapezoidal drive.
The sinusoidal drive current waveform follows a sinusoidal like pattern in which ripples
and audible noise are reduced.
Figure 2. Phase Current