The Find window is outside the SmartDesign canvas, but can be used to easily find design objects
to make net connections.
- 1.Open the SmartDesign component in the canvas.
- 2.Click Edit >
Find in the Libero SoC menu to open the Find window at the bottom of
the Libero main window.
- 3.In the Search
menu, select Current Open SmartDesign.
- 4.Enter the type of design objects
(Instance/Net/Pin) from the Type menu.
- 5.Enter the string of characters in the
Find box.
- 6.Click Find All.
- 7.If there are matches, click the item
in the Search Results.
The SmartDesign canvas zooms in and highlights the design object. Zoom out far enough, with the
design object still selected, to see the rest of the design and make the net
connections.