If the instance is a SmartDesign component, the Configure action opens the SmartDesign canvas for edits. If the selected instance is an IP or HDL Core, the Configure button opens the Configurator dialog box for the core to be configured. If the selected instance is an HDL, the configure action opens the HDL file in the text editor. This action is equivalent to double clicking the instance. This action is available only when one single instances is selected.