This menu item is available to instance pins. If a group is selected first, right click a pin and choose Add Pin to Group to add the pin to the selected group. If no group is selected first, the menu item is called Add Pin to New Group, a new group with the default group name Group/Group_1/Group_2/Group_3/ and so on is created, and all selected pins are added to the newly created group.
A pin group can be expanded to display the member pins or collapsed to hide the member pins. Member pins connected to nets cannot be hidden and cannot be collapsed into the group. Only member pins (in a pin group) with Pin Attributes (Tie high/low/marked unused) can be hidden and collapsed into the pin group.