Working in SmartDesign
1.
How do I make manual connections?
2.
How do I connect a pin to the top level?
3.
Oops, I just made a connection mistake. How do I disconnect two pins?
4.
I need to apply some simple 'glue' logic between my cores. How do I do that?
5.
My logic is a bit more complex than inversion and tie offs - what else can I do?
6.
How do I create a new top-level port for my design?
7.
How do I rename one of my instances?
8.
How do I rename my group pins?
9.
I need to reconfigure one of my Cores, can I just double click the instance?
10.
I want more Canvas space to work with!
Parent topic:
Appendix A - FAQ