This option opens a dialog box for entering a list of slices. If these slices are all valid, they
are added to the bus. If the slices are not valid (for example, slice bits already exist
and used in an existing slice), the error is reported in the Log window. The dialog box
supports any separator character except colon because the colon is used to specify a
range. No characters other than the colon are allowed to be adjacent to the two-range
indices.
Note: Creating a custom slice
does not delete pre-existing slices.
Figure 1. Custom Slices Dialog Box