The SWD interface on the
WLR089U0 module is
supported by Microchip’s programmers and debuggers like Atmel-ICE, SAM-ICE™ and an
on-board Embedded Debugger in the WLR089 Xplained Pro. It is also supported by several
third-party programmers and debuggers. For programming and/or debugging the
WLR089U0 module:
- 1.Connect the Programmer/Debugger
with the module using the Serial Wire Debug (SWD) interface.
- 2.Select the Device as WLR089U0.
Notes: For more details, refer the following
documents:
- For Programming and Debugging,
refer to the Atmel-ICE, SAM-ICE or WLR089 Xplained Pro Board User
Guide.
- For Microchip, third-party
programmers and third-party programming houses, refer to the AN2468
Production Programming of Microchip AVR® and SAM Microcontrollers
Application Note (DS00002468).
- Connecting to any other
programming or debugging tool, refer to that specific programmer’s guide or
debugger’s user guide.