AT32UC3CB1256 Default Firmware Configuration
The default firmware pre-loaded on the Atmel AT32UC3B1256 is dynamically configurable upon power-up:
The USB DFU Bootloader can be enabled by closing the J28 jumper
Use FLIP/batchisp to read/write resources on the AT32UC3B1256 through the bootloader
Programming the AT32UC3B1256 will overwrite the default firmware.
Test points
A few test points covering the USB Interface block have been placed on the Atmel AT32UC3C-EK for the verification of important signals.
Designation | Feature |
---|---|
TP64 | VBUS |
TP65 | D- |
TP66 | D+ |
TP67 | GND |
TP68 | JTAG.TCK.UC3B |
TP69 | JTAG.TDO.UC3B |
TP70 | JTAG.TMS.UC3B |
TP71 | JTAG.TDI.UC3B |
TP72 | RESET_N.UC3B |