In MPLAB® X v6.05, launching MPLAB® Code Configurator (MCC) in projects previously configured using MCC Classic will result in an error where the contents of the GUI components in the Easy Setup interface will appear blank, similar to the screen captures below:
This issue only appears when using MPLAB® X v6.05 and only for MCC projects previously configured in MCC Classic, using MPLAB® X v6.00 or earlier.
To fix the issue, users must update the project to use the latest MCC Core version and/or the latest versions of their library. Update steps vary depending on the MCC Core version used to configure the project and if the modules involved are System/Peripheral Modules or Library/Driver Modules.
If the project is already using the latest available MCC Core, skip to Updating Module Versions Using Content Manager.