There are two kinds of cables, which can be used to connect the Atmel-ICE kit to AVR or SAM chip programming interface pins, as shown in the figure below, provided in the full kit:
For most purposes, the 50-mil 10-pin IDC flat cable can be used, connecting either natively to its 10-pin or 6-pin connectors, or connecting via the adapter board, as shown in the figure below. Three adapters are provided on one small PCBA. The following adapters are included:
To assemble your Atmel-ICE into its default configuration, connect the 10-pin 50-mil IDC cable to the unit, as shown in the figures below. Be sure to orient the cable so that the red wire (pin 1) on the cable aligns with the triangular indicator on the blue belt of the enclosure. The cable should connect upwards from the unit. Be sure to connect to the port corresponding to the pinout of your target, AVR or SAM.