Synchronous Master Transmission Setup
- 1.Initialize the SPxBRGH, SPxBRGL register pair and the BRG16 bit
to achieve the desired baud rate (see EUSART Baud Rate Generator (BRG)).
- 2.Select the transmit output pin by writing the appropriate values to the RxyPPS register
and RXxPPS register. Both selections should enable the same pin.
- 3.Select the clock output pin by writing the appropriate values to the RxyPPS register
and CKxPPS register. Both selections should enable the same pin.
- 4.Enable the synchronous master serial port by setting bits SYNC, SPEN and CSRC.
- 5.Disable Receive mode by clearing bits SREN and CREN.
- 6.Enable Transmit mode by setting the TXEN bit.
- 7.If 9-bit transmission is desired, set the TX9 bit.
- 8.If interrupts are desired, set the TXxIE bit of the PIEx
register and the GIE and PEIE bits of the INTCON register.
- 9.If 9-bit transmission is selected, the ninth bit should be loaded in the TX9D bit.
- 10.Start transmission by loading data to the TXxREG register.
Figure 1. Synchronous Transmission