The following steps are a guide to program the firmware build through the ASF project
using Microchip Studio.
- 1.In Microchip Studio, go to the
Tools tab to program the HEX files into the SAML21. Select Device
Programming or press Ctrl+Shift +P.
Figure 1. Options in
Tools Tab
- 2.In the Device Programming window,
select the corresponding EDBG, and click Apply.
Figure 2. Device
Programming Window
- 3.In the EDBG Device Programming
Window, go to the Memories tab and browse .Hex file as shown in the
following figure:
Figure 3. EDBG Device
Programming Window
- 4.Click Program for the tool
to program SAML21. The following figure illustrates the status of programming.
Figure 4. Program Option
in EDBG Device Programming Window