Using the Embedded Debugger on the ATmega328P
Xplained Mini board to program the ATmega328P.
- 1.Connect the Xplained Mini USB to
the PC.
- 2.Go to Atmel Studio: Click the
Tools tab, select Device Programming, and select the connected mEDBG as Tool
with Device as ATmega328P and
Interface to ISP, click
Apply.
- 3.Select “Memories”, locate the
source .hex or .elf file, and click Program.
- 4.NOTE: If a previous debug
session was not closed by selecting “Disable debugWIRE and Close” in the Debug
menu, the DWEN fuse will be enabled, and the target will still be in debug mode,
i.e., it will not be possible to program the target using the ISP interface.
- 5.If the source file contains fuse
settings, select “Production file” and upload the .elf file to program the
fuses.
- 6.Select “Fuses” to program the fuses
manually. Set the fuse(s) and click “Program”. Recommended fuse settings: