Todo: Configure
the Event system in Atmel | START.
- 1.Select Re-Configure Atmel Start
Project by right-clicking the ADC_Training project in the Solution
Explore window from the previous assignment.
- 2.Add in the Events System component
in the opened Atmel | START window:
- 2.1.Expand the driver from the ADD
SOFTWARE COMPONENT window by clicking
in the
Atmel | START window.
- 2.2.Select the Events System driver
by clicking
.
- 2.3.Add in the selected Events
System component by clicking
.Info: The
Events System driver will be added to the project.
- 3.Configure the Asynchronous Event Channel 0
as shown in Figure 1.
Figure 1. Event Source Selection
- 3.1.Select the EVENTS icon on the
left side of the window.
- 3.2.Select Asynchronous Event Channel
0.
Info: The EVENT SYSYEM SETTINGS window
should appear.
- 3.3.Scroll down and select the Real Time
Counter overflow option in the popped up EVENT SYSTEM SETTINGS window and
close the window.
- 4.Configure the Event user as shown in Figure 2:
- 4.1.Click the setting dialog under USERS
-> ADC0.
- 4.2.Select the checkbox of Start Event
Input Enable in the popped up EVENT SYSTEM SETTINGS window.
- 4.3.Select Asynchronous Event Channel
0 as ASYNCUSER1 in the popped up EVENT SYSTEM SETTINGS window and close the
window.
Figure 2. Event Channel Selection
Info: The
Event system configuration is now completed with the event generator, event channel, and
event user defined as shown in
Figure 3.
Figure 3. Event User Selection
![](GUID-04FBB75F-5AC6-453C-AA04-DB7DC260D600-low.jpg)
- 5.Reconfigure RTC in Atmel | START:
- 5.1.Reopen the RTC configuration window by
clicking DASHBOARD on the left side of the window.
- 5.2.Click the existing RTC_0
module.
- 5.3.Unselect the checkbox for OVF:
Overflow Interrupt enable as marked with red in Figure 4.
Figure 4. RTC Reconfiguration
- 6.Regenerate the project by clicking the
GENERATE PROJECT button. The project summary window pops up. Click OK.