Add RTC Driver in
Atmel | START
Add RTC drivers to the project in
Atmel | START
with the following steps:
1.
Select the project by right-clicking the
ADC_Training
project in the
Solution Explorer
window from the previous assignment.
2.
Reconfigure the project by clicking the
Re-Configure Atmel | START Project
option in the menu as shown in
Figure 1
.
Figure 1.
Reconfigure Atmel | START
Info:
The
Atmel | START
window should appear within
Atmel Studio
.
3.
Add the RTC component in
Atmel | START
:
3.1.
Expand
Drivers
from the
ADD SOFTWARE COMPONENT
window by clicking
in the
Atmel | START
window.
3.2.
Select
RTC
by clicking
as shown in
Figure 2
.
Figure 2.
Add RTC Component in Atmel | START
3.3.
Add the selected RTC component by clicking
.
Info:
The RTC module will be added to the
ADC and Power Optimization
project.
Parent topic:
Assignment 2: RTC Interrupts Triggers ADC and USART Print