Once the ADC and USART functional drivers have been added using Atmel | START, developing the application code can be started.
Todo: Add code to
the application which performs ADC conversion and sends the ADC result via USART to a
terminal.
- 1.Include functions for adding delays to the
application code by adding the following line of code at the beginning of
main.c.
#include <util/delay.h>
- 2.Add ADC and USART functionality to the
application, by adding the following piece of code in the
while(1)
-loop in
the main
function.
ADC_0_start_conversion(10); //Start ADC conversion on channel 10
while(!ADC_0_is_conversion_done()); //wait for ADC conversion is done
USART_0_write(ADC_0_get_conversion_result()); //USART write ADC result
while(!(USART0.STATUS & USART_TXCIF_bm)); //wait for USART TX complete
_delay_ms(500); // delay to easier observe changes to ADC input in terminal
Info: main.c
should look similar to the code in
Figure 1
Figure 1. main.c Code
- 3.Go to the implementation of ADC_0_start_conversion() by
- 3.1.Hover over ADC_0_start_conversion().
- 3.2.Right-click → Goto Implementation
Info: A menu,
showing the different locations, will appear.
- 3.3.Jump to where the function is
implemented by selecting the first option from the pop-up window.
Info: The implementation of
ADC_0_start_conversion(), which is located in
adc_basic.c, should now be visible in the Atmel Studio editor
window.
- 4.View the complete list of ADC driver functions by clicking the arrow, shown in Figure 2.
Figure 2. ADC Driver Function List
Info: The ADC driver functions marked with 2-5 in
Figure 2 are all used by this training.
- 5.Go to the implementation of USART_0_write() by
- 5.1.Hover over USART_0_write() in the main.c file.
- 5.2.Right-click → Goto Implementation
Info: A menu,
showing the different locations, will appear.
- 5.3.Jump to where the function is
implemented by selecting the first option from the pop-up window.
Info: The implementation of
USART_0_write(), which is located in
usart_basic.c should now be visible in the
Atmel Studio editor window,
as shown in
Figure 3.
Figure 3. USART Driver Function
List
Info: USART_0_write is the only USART driver function used
in this training.
Result: Adding ADC
and USART functionality to the application code is completed.