This training contains five hands-on applications doing ADC data conversion, with current consumption measured for each application. The training starts with a simple ADC conversion application. In the following applications, different techniques have been introduced in order to demonstrate how the current consumption can be reduced.
This training will also demonstrate how to use Atmel | START to get started with AVR® ADC applications development. The ADC applications have been developed step-by-step in Atmel Studio. This training has been developed on the ATtiny817 Xplained Pro evaluation kit, but should apply for all tinyAVR® 0- and 1-series, and megaAVR® 0-series devices.