Once the application code has been developed and the hardware has been set up, it
is time to run the application and to set up Data Visualizer in order to observe the ADC
functionality and the power measurement.
Todo:
- Set up the Data Visualizer
terminal in Atmel Studio to display the ADC data transmitted from the
evaluation kit via the EDBG Virtual COM Port, and observe the ADC functionality.
- Set up the power analysis in Data
Visualizer and observe the microcontroller's current consumption in Data
Visualizer.
- 1.Open the Data Visualizer in Atmel Studio by clicking Tools → Data
Visualizer.
- 2.Connect ATtiny817 Xplained Pro to Data Visualizer, refer to Figure 1, by
- 2.1.Open Serial Port Control Panel by clicking Configuration → External
Connection → double-click Serial Port.
- 2.2.Select ATtiny817 Xplained Pro's
Virtual COM port by selecting EDBG Virtual COM Port from the drop-down list.
Tip: The EDBG Virtual COM Port
number associated with the ATtiny Xplained Pro kit can be found in Windows Device
Manager by clicking: Start → Control Panel → Device Manager →
Ports.
- 2.3.Set the Baud rate to 96000 in the Baud rate field.
- 2.4.Open the terminal window by clicking Connect in the Serial Port Control
Panel.
Figure 1. Connect to Data Visualizer
- 3.Ensure human-readable print-out from the
terminal window, by selecting Hexadecimal Values, see Figure 2
- 4.Observe the ADC functionality by seeing how
the values in the terminal window changes as the potmeter knob is rotated, as shown in Figure 2.
Figure 2. ADC Results in Terminal
Window
Info: As
the ADC resolution has been configured to 8 bits, the ADC result printed to the terminal
window will range from 0x00 to 0xFF, when the potentiometer knob is rotated.
- 5.Open the Power Analysis window in
Data Visualizer, as shown in Figure 3, by
- 5.1.Connect ATtiny817 Xplained Pro
to the data gateway interface by clicking Connect in DGI Control Panel by
pressing the Connect button.
Info: This button will show as
Disconnect once ATtiny817 Xplained Pro is connected.
- 5.2.Enable for power data being sent from
ATtiny817 Xplained Pro to the data gateway interface by selecting Power
in DGI Control Panel.
- 5.3.Start receiving data through the data
gateway interface by clicking Start.
Figure 3. DGI Control Panel
Info: A
Power Analysis window should appear in Data Visualizer.
- 6.Observe the current consumption for
ATtiny817 in Power Analysis, as shown in Figure 4.
Figure 4. Power Analysis Window
Info: As
shown in
Figure 4, the average current consumption of
ATtiny817 is
around 2.8 mA, with small variations when rotating the potentiometer knob.
Note: The power consumption may vary depending on
the value of the potentiometer connected (e.g. the current consumption can be 2.1 mA with
another potentiometer). The power consumption measured in the following assignments could
also vary slightly.
Info: The power consumption is high compared to
the performance of ATtiny817. The following assignments will use different
techniques which will reduce the power consumption.
Result: By
connecting ATtiny817 Xplained Pro to Data Visualizer one can easily observe the
ADC functionality through a terminal window, and by using the current measurement features of
ATtiny817 Xplained Pro, the device's consumption can be observed.