In order to use the 16-bit language tools with MPLAB X IDE, you must install:
The 16-bit language tools will be installed, by default, in the directory:
C:\Program
Files\Microchip\xc16\x.xx
C:\Program Files
(x86)\Microchip\xc16\x.xx
Applications/microchip/xc16/x.xx
/opt/microchip/xc16/x.xx
where x.xx
is the version number.
The executables for each tool will be in the bin
subdirectory:
xc16-gcc.exe
xc16-as.exe
xc16-ld.exe
xc16-ar.exe
xc16-utility.exe
Device support files may be found under the support
subdirectory. The generic xc.h
C header file and xc.inc
generic assembler include file may be found under the support/generic
subdirectory.