The expected start-up sequence for the MPLAB PICkit 4 debugger is:
The indicator light strip has the following significance.
Color | Description |
---|---|
Blue | Power is connected; debugger in standby. |
Orange | Power target circuit from PICkit 4 checked. |
Green | Power target circuit from PICkit 4 unchecked. |
Red | Lit when the debugger has failed. |
The following tables provide descriptions of the indicator lights and bootloader errors.
Color | Description |
---|---|
Blue | Power is connected; debugger in standby. |
Orange | Power target circuit from PICkit 4 checked (see Table 1). |
Green | Power target circuit from PICkit 4 unchecked (see Table 1). |
Purple | Bootloader is running. |
Yellow | Debugger is busy. |
Red | An operation has failed. |
Purple | Fast blink indicates the time window for forcing the debugger into Bootload mode. |
Bootloader Errors | Description |
---|---|
Red, slow blink | Power accessing the debugger’s serial EEPROM. |
Red, fast blink | Bootloader API commands cannot be processed. |
White, fast blink | A runtime exception occurred in the tool firmware. |