If the MPLAB X IDE or MPLAB IPE cannot communicate with the debugger, the debugger may need to be forced into bootload mode (download new firmware). Some possible reasons could be the following:
This can occur if the Project Properties Firmware options has the “Use Latest Firmware” box unchecked and there is a new firmware version available with the MPLAB X IDE version.
In this case, check the “Use Latest Firmware” box and click the Refresh Debug Tool Status Icon in the MPLAB X IDE dashboard display. If there is still an asterisk next to the Application version number, or the debugger issue is not resolved, proceed to the following steps for bootload mode.
Also, refer to Indicator Lights Strip for more information on light strip modes and bootloader errors.
Perform the following steps to force the debugger into bootload mode: