If the MPLAB PICkit 4 In-Circuit Debugger
and MPLAB X
IDE or MPLAB IPE are not communicating with
each other:
- 1.Unplug and then plug in the debugger.
- 2.Reconnect to the debugger.
- 3.Try the operation again. It is possible the error was a one-time event.
- 4.The version of MPLAB X
IDE or MPLAB
IPE installed may be incorrect for the version of firmware loaded on theMPLAB PICkit 4 In-Circuit Debugger. Follow the steps
outlined in Corrupted Installation Actions.
- 5.There may be an issue with the computer USB port. See section USB Port Communication Error Actions.