Debugger options are set in the Project Properties dialog. Click on PICkit 4 under Categories to display the Options for PICkit 4 (see figure below). Use the Options categories drop list to select various options. Click on an option name to see its description in the Option Description box below. Click to the right of an option name to select or change it.
After setting the options, click Apply or OK. Also click the Refresh Debug Tool status icon in the MPLAB X IDE dashboard display to update any changes made.