Select the Programmer-To-Go options.
Image Name | The default image name is “<your project name>_ptg,” though you can edit the name if you wish. This will be the folder name on the microSDHC card that contains the appropriate files for Programmer-To-Go. |
Send image to tool | This check box is selected by default. With the box checked, the PTG image is created and then sent to the microSDHC card in the connected MPLAB PICkit 4. |
Program Device | This check box is selected by default. With the box checked, the device connected to the MPLAB PICkit 4 is programmed. |