Using MPLAB IPE, follow these steps to download the project files
into the microSDHC card in the MPLAB PICkit
4 and enter Programmer-To-Go mode.
- 1.Insert a formatted
FAT32-compatible microSDHC card into the PICkit. 4.
- 2.Ensure that you have the appropriate connections to the device for
Programmer-To-Go:
- PICkit 4
is connected to the computer via the USB cable.
- PICkit 4
is connected via the appropriate programming
interface connector to the target board.
- The
target board is powered from either the PICkit 4 or
a power supply, depending on your Project Properties
selection.
- 3.From the MPLAB IPE menu,
select Settings, Advance Mode and type in the password
to log in. Click the Settings icon on the left to open the
Special Setting dialog and locate the Programmer-To-Go settings.
Figure 1. MPLAB
IPE Programmer-To-Go Options
- 4.In the Image Name
field, the default is “<your project name>_ptg,” though you
can edit the name if you wish. This will be the folder name on the
microSDHC card that contains the appropriate files for
Programmer-To-Go.
- 5.In the Send image to
tool, the check box is selected by default. With the
check box selected, the PTG image is created and then sent to the
microSDHC card in the connected MPLAB PICkit
4.
- 6.The Program Device
the check box is selected by default. With the box checked, the
device connected to the MPLAB PICkit
4 is programmed.
- 7.Click the
Programmer-To-Go button.
During this process, the device is programmed, then the Programmer-To-Go
directory is populated with the appropriate files for the
Programmer-To-Go operation into the microSDHC card. The
Output window displays a status message “Programming/Verify
complete” when the process finishes successfully.
Note: The
PTG settings on the microSDHC card are the same as
in the project (for example, memory, power,
etc.).
The PICkit 4 is now in
Programmer-To-Go mode. The LED should blink
green to indicate the tool has been configured successfully
for Programmer-To-Go.
- 8.Disconnect the PICkit 4
and you’re ready to use Programmer-To-Go.