Note: For information on programming, refer to the MPLAB X
IDE
online Help.
Attention: MPLAB PICkit
4 does not support debug headers.
In MPLAB X
IDE, use the MPLAB PICkit
4 as a programmer to program a non-ICE/-ICD
device, such as a device not on a header board. Set the MPLAB PICkit 4 In-Circuit Debugger as the current tool (click the Debug Tool PICkit 4 in the
navigation window, select File > Project Properties, then under “Hardware
Tool,” click PICkit 4 to perform these actions:
- When Run Main Project icon (see below) is selected, the application
code is programmed into the device’s memory via the ICSP protocol. No clock is required
while programming and all modes of the processor can be programmed – including code
protect, Watchdog Timer enabled, and table read protect.
Figure 1. Run Main Project Icon
- A small “program executive” program may be loaded into the high area
of program memory for some target devices.
- Special “in-circuit debug” registers in the target device are disabled
by MPLAB X
IDE, along with all debug features. This means
that a breakpoint cannot be set and register contents cannot be seen or altered.
- The target device is run in Release mode. As a programmer, the
debugger can only toggle the MCLR line to
Reset and start the target device.
The MPLAB PICkit 4 In-Circuit Debugger system
programs the target using ICSP. VPP, PGC and PGD lines should be connected as
described previously. No clock is required while programming and all modes of the processor
can be programmed, including code protection, Watchdog Timer and table read protection.