Use the Project Properties dialog to select or switch debuggers for a
project. To switch you must have more than one debugger connected to your computer. MPLAB X
IDE will differentiate between the debuggers by
displaying different serial numbers.
To select or change the debugger used for a project:
- 1.Open the Project Properties dialog by doing one of the following:
- a.Click on the project name in
the Projects window and select File > Project
Properties.
or
- b.Right
click on the project name in the Projects window and
select Properties.
- 2.Under Categories on the left
side, expand “Conf:[default]” to show PICkit 4.
- 3.Under Hardware Tools, find
PICkit 4 and click on a serial number (SN) to select a debugger for use
in the project, then click Apply.