CheckMac
CommandThe CheckMac
command calculates a MAC response that would
have been generated on a different CryptoAuthenticationâ„¢ (ECC608, ATECC508A, ATSHA204A) device and then compares the result with the
input value. The command returns a boolean result to indicate the success or failure of
the comparison.
If a value in TempKey is used as an input to the CheckMac
,
then a Nonce
and/or GenDig
command must be run prior
to the CheckMac
command.