ECC private keys are the fundamental building blocks of ECC Security. These keys are private and unique to each device and can never be read. ECC private keys are randomly generated by the secure element's TRNG and are securely held in slots configured as ECC private keys.
There are additional private keys that can be used for future use cases, such as additional service authentication.
These keys are enabled for the following primary elliptic curve functions:
Secondary private keys can be overwritten with a new internally-generated
private key (GenKey
) to enable key deletion, key rotation and
remote provisioning. The keys are also slot-lockable (KeyConfig.Lockable bit is set
to zero), meaning the Lock
command can be used in SlotLock mode to
render the current key permanent and prevent it from being changed by the
GenKey
command. When performing key changes, Key Attestation is required
to ensure to another system that the device’s new public key being presented
actually originated from the device in question.
The private key in slot 1 is configured as an internal sign-only key, which means it
can only sign messages generated internally by the GenKey
or
GenDig
commands and cannot be used to sign arbitrary external
messages. This feature allows the internal sign key to be used to attest to what
keys are in the device and their configuration/status to any system that knows (and
trusts) the internal sign public key.