Counter Command

The Counter command reads the binary count value from one of the two monotonic counters located on the device within the Configuration zone. The maximum value that the counter may have is 2,097,151. Any attempt to count beyond this value will result in an error code. The counter is designed to never lose counts even if the power is interrupted during the counting operation. In some power loss conditions, the counter may increment by a value of more than one.

For the ECC608-TNGHNT, the counters are not attached to any keys but may still be used by the system. Each count is set to its default value and can count to the maximum value.