This file contains function prototypes and other datatypes for CPU self tests.
This enumeration indicates the operating mode in which the DIAG_CPU_SelfTest diagnostic API function will be executed.
Execute Subset-1 function within the current execution of the diagnostic API function. | |
Execute Subset-2 function within the current execution of the diagnostic API function. | |
Execute Subset-3 function within the current execution of the diagnostic API function. | |
Execute all Test Subset functions sequentially within the current execution of the diagnostic API function. In this mode, only one invocation of the function is sufficient to fully perform the diagnostic function. |
[in] executionMode |
diag_cpu_execution_mode_t Enum
- indicates the operating mode in which the DIAG_CPU_SelfTest diagnostic API function will be executed |
uint8_t | 8-bit Error Mask <- - - - - S3 S2 S1>. Test bit = 1: Subset execution is successful; Test bit = 0: Subset execution is failed. |