This file contains API prototypes for Indirect Time-Slot Monitoring based WDT Test (Simple-Timer Mode)
The following is an UML Test State diagram for SW_WATCHDOG_SIMPLE_TIMER_STARTUP_TEST_01: .
This enum has the valid status for the WDT test.
This enum is used to show if the backup of the RSTFR register is valid.
0 - is assigned to WDT Test State in case of faults | |
1 - is assigned to WDT Test State to perform WDT Simple Timer Test | |
2 - is assigned to WDT Test State on error-free execution of |
0 - indicates that the WDT functionality is error-free | |
1 - indicates that WDT functionality has failed |
0 - indicates that the backed up RSTFR register is not corrupted | |
1 - indicates that the backed up RSTFR register is corrupted |
void |
void | See DIAG_WDT_SimpleTimer_GetStatus() |
void |
diag_simple_wdt_status_t | DIAG_WDT_SIMPLE_PASS, DIAG_WDT_SIMPLE_FAIL |
[in] store_RSTFR_copy_p |
uint8_t * |
diag_RSTFR_backup_status_t | DIAG_RSTFR_BACKUP_OK, DIAG_RSTFR_BACKUP_ERROR |