This enumeration indicates the operating mode in which the DIAG_CPU_SelfTest diagnostic API function will be executed.
Execute Subset-1 function within the current execution of the DIAG_CPU_SelfTest diagnostic API function. | |
Execute Subset-2 function within the current execution of the DIAG_CPU_SelfTest diagnostic API function. | |
Execute Subset-3 function within the current execution of the DIAG_CPU_SelfTest diagnostic API function. | |
Execute all Test Subset functions sequentially within the current execution of the DIAG_CPU_SelfTest diagnostic API function. In this mode, only one invocation of the DIAG_CPU_SelfTest function is sufficient to fully perform the diagnostic function. |