This file contains APIs for Interrupt Frequency test.
Parameters |
|
||||
Returns |
|
void |
void | None |
[in] intrId |
diag_interrupt_id_t
- ID for interrupt to be monitored |
[in] refCount |
uint16_t
- The expected number of interrupts within monitoring period |
[in] tolerance |
uint16_t
- Limit for deviation in the counter |
[in] ftti |
uint16_t
- Count which when reaches zero checks the interrupt frequency. If fttiCount is non-zero, that means the interrupt frequency check should be skipped for that instance and intr_counter should not be incremented |
bool | bool |
[in] intrId |
diag_interrupt_id_t
- ID for the interrupt to be unregistered |
bool | bool |
[in] intrId |
diag_interrupt_id_t
- ID for the interrupt to be updated. |
void | None |
void |
void | None |
[in] intrId |
diag_interrupt_id_t
- ID of the interrupt for which test status is requested. |
diag_interrupt_test_status_t | DIAG_INTR_PASS - Success, DIAG_INTR_FAIL - Failure, DIAG_INTR_INVALID - Indeterminate |