diag_interrupt_params_t Struct
This is the interrupt model structure that is used in the DIAG_INTERRUPT_Frequency. Initially, for each interrupt that is registered and to be monitored for the frequency test, the structure parameters are initialized as specified in DIAG_INTERRUPT_Register API. Later, when test is running, structure elements will be continuously updated to hold the actual values to be used to evaluate the test.