Initializes a Generic Clock Generator configuration structure to defaults.
void system_gclk_gen_get_config_defaults( struct system_gclk_gen_config *const config)
Initializes a given Generic Clock Generator configuration structure to a set of known default values. This function should be called on all new instances of these configuration structures before being modified by the user application.
Clock is generated undivided from the source frequency
Clock generator output is low when the generator is disabled
The input clock is sourced from input clock channel 0
Clock will be disabled during sleep
The clock output will not be routed to a physical GPIO pin
Data direction | Parameter name | Description |
---|---|---|
[out] |
config |
Configuration structure to initialize to default values |