You can test the presence of the 32-kHz crystal clock by redirecting the clock to an
external GPIO. Two actions are possible, depending on the customer application:
- Redirect the 32-KHz clock to
PC15
- Redirect the 32-KHz clock to
PC31
Before it is run, the script must be adapted to the selected customer UART console.
One of the following files must be updated as required by the
Customer UART Console Configuration:
- SAM9X60D1G_32KHz_PCK0_Generation.bat when PC15 GPIO is used for clock
redirection
- SAM9X60D1G_32KHz_PCK1_Generation.bat when PC31 GPIO is used for clock
redirection
Both files are available in the folder "%DIR_PATH%\SOFTWARE\". They must be updated
according to requirements as follows:
- 1.Open the file
"SAM9X60D1G_32KHz_PCK0_Generation.bat" or "SAM9X60D1G_32KHz_PCK1_Generation.bat"
using a text editor.
- 2.On line 20, add the comment "rem"
at the beginning of the line. This selection is the default configuration and
must be commented out to enable the case.
- 3.Remove the comment "rem" on the
line with the selected FLEXCOM/IOSET.
- 4.Save and close the file. No
compilation is required.