Before it is run, the script must be adapted to the selected customer UART console.
The file "SAM9X60D1G_DDR2_Check.bat" available in the folder "%DIR_PATH%\SOFTWARE\" must
be updated as required by the Customer UART Console Configuration.
- 1.Open the file
"SAM9X60D1G_DDR2_Check.bat" with a text editor.
- 2.On line 20, add the comment "rem"
at the beginning of the line. This selection is the default configuration and
must be commented out to enable the case.
- 3.Remove the comment "rem" on the
line with the selected FLEXCOM/IOSET.
- 4.Save and close the file. No
compilation is required.