If the USB device is not recognized by the operating system, the driver must be updated
as follows:
- 1.Go to “Device Manager” in the
control panel.
- 2.Select the properties of the
“Unknown Device” that appears when the USB device is connected.
- 3.Update the driver by selecting
the file “atm6124_cdc.inf” available in the folder
%DIR_PATH%\SOFTWARE\driver\.
The figure below shows how the interface is shown to the operating system.