To perform the GPIO toggling test, a specific qml file (GPIO-Toggling-usb.qml) is
required and available in the following folder:
- %DIR_PATH%\SOFTWARE\tests\GPIO
Before launching the script, the user must make sure, depending on the customer's GPIO
configuration, that the I/O toggling will not affect the reliability and/or operability
of the customer's application.
To change the GPIO list, open the "GPIO-Toggling-usb.qml" file using a text editor and
adapt the GPIO list as required. The qml script can be adapted as follows:
- Adapt the "output_pio_array"
table:
- Apply "0" when you select
PIO from the PIOA bank.
- Apply "1" when you select
PIO from the PIOB bank.
- Apply "2" when you select
PIO from the PIOC bank.
- Apply "3" when you select
PIO from the PIOD bank.
- Adapt the "output_pin_array"
table
- Apply the number
corresponding to the PIO number (e.g. 25 for PA25).
- Adapt the
"number_of_toggling_cycle" variable as required.
- Adapt the "number_of_io_toggling"
variable. The applicable value is the number of I/Os listed in the two tables
above.
- Adapt the "delay_time" variable
as required.
Save and close the file. No compilation is required.
The following is a toggling function example for the PB11, PB12 and PB13 PIOs.