Failure Analysis

The following procedure can be applied in case of failure analysis.

Notes:
  1. 1.Important: the system must not boot on an external memory before the module is powered up. For more details, see Embedded Software Prerequisites.
  2. 2.If the device is not recognized by the operating system, the system driver must be updated. See Updating the Windows Driver.
  3. 3.To perform PMIC voltage measurements, refer to the figure below.